How to change GMT Time Zone on the DX4700/4800 HVR Recorder.

Issue

How to change GMT Time Zone on the DX47/4800 HVR Recorder.

Product Line

Pelco Video Management

Environment

  • DX4700/4800 HVR Recorder.

Cause

The time zone is configured for GMT 0 by default.

Resolution

 

  1. Click the   icon on the toolbar and login with the 'admin' account.





     
  2. To access the Setup window, on the toolbar, click on the Setup Icon .
     
  3. Select the System menu using the directional arrows or mouse.
     
  4. Select Date/Time.
     
  5. Edit the GMT time zone for your location.
     
  6. Click the X in the upper right corner to close, when prompted select OK to save.


    Note: Click here for view of the Setup Window page.

     

Related Articles:
What is the default username and password for the DX4700/DX4800 Series HVR?