Which wall mounts are recommended for the IS20 camclosures?

Issue

Which wall mount can I use with the IS20 camclosures?

Product Line

Pelco Cameras

Environment

  • IS20 series
  • IS20-P

Cause

Recommended mounts

Resolution

IS20 pendant mounts: