Can I disable the login request on Spectra IV IP using the TXB-IP

Issue

The desire to view Live video thru a web browser without logging in cannot be established using the TXB-IP encoder board (an Atlas) product.

Product Line

Pelco Cameras

Environment

  • ALL IP cameras using Atlas (Non Sarix firmware.)
  • TXB-IP
  • Spectra IV IP Mpeg4
  • IP3701
  • IP110

Cause

  • The firmware was purposely set up to require a login for viewing LIVE video. It would require a codec change.

Resolution

Use the TXB-N series encoder board.