Warning
Electrostatic Discharge Required: Always discharge static electricity from your person by touching metal prior to handling any hardware. Failure to do so may result in damage to devices.
Issue
Battery power on an MN50-RTC is low and needs to be replaced.
Product Line
Satchwell MicroNet
Environment
- Controller PCB
- Power supply
- Timeclock
Cause
Low power in battery
Resolution
The replacement battery is a standard CR1632 3 volt 125mAh
Updated January 2014.
The MicroNet 50 series range MN350,450,550,650 LCD and Touchscreen have been withdrawn from sale.
Currently no direct replacement is offered.