Does the ICS100 take 24 VAC or 12VDC?

DANGER

HAZARD OF ELECTRIC SHOCK.
Remove all power from all devices before removing any covers or doors of the system. Disconnect the power at the device and at the power source.

WARNING

ELECTROSTATIC DISCHARGE REQUIRED.
Discharge all static electricity from your person by touching metal prior to handling any hardware. Failure to do so may result in damage to devices.

Issue

Does the ICS100 take 24 VAC or 12VDC?

Product Line

Pelco Cameras

Environment

ICS100 series

Cause

Need to set the ICS100 to 24VAC.

Resolution

The ICS100 can take either 24 VAC or 12 VDC, the selection is made according to the jumper placement.