NVR5100 Network Video Recorder showing a PXE error then exits the boot agent.

DANGER

HAZARD OF ELECTRIC SHOCK.
Remove all power from all devices before removing any covers or doors of the system. Disconnect the power at the device and at the power source.

WARNING

ELECTROSTATIC DISCHARGE REQUIRED.
Discharge all static electricity from your person by touching metal prior to handling any hardware. Failure to do so may result in damage to devices.

Issue

NVR5100 Network Video Recorder will not boot and will not recognize the computer keyboard.

Product Line

Pelco Video Management

Environment

  • NVR5100 Network Video Recorder all versions

Cause

The NVR5100 Network Video Recorders RAM or VGA card has come lose.

Resolution

Remove the NVR5100 Network Video Recorders cover and re-seat the VGA card and RAM.