PDA will not connect to the Spectra IV 36X Dome Drive.

Issue

The PDA used to service the Spectra III and Spectra IV series systems will not interface with the 36X models of the Spectra IV series.

Product Line

Pelco Cameras

Environment

  • DD436
  • SD436
  • SD4E
  • SD4N
  • Palm 1 Tungston E2  PDA

Cause

The Spectra IV 36X is not compatible with the PDA.

Resolution

To connect to the Spectra IV 36X dome drives:

  1. The IPS-CABLE is needed
  2. PC running Windows XP, Vista, Windows 7 32/64 bit.
  3. Downloader II Software Version 2.2.12

Download the Software: Downloader.2.2.12.zip

See related Lessons Learned article: