How to specify the number of digits to display after the decimal point in a Pinpoint Graphic.

Issue

How to specify the number of digits to display after the decimal point in a Pinpoint Graphic.

Product Line

Andover Continuum

Environment

CyberStation

Cause

Have Graphic that is displaying a temperature value as 78.567, customer wants the temperature displayed with only ONE decimal place (78.56)

Resolution

PinPoint graphics display the value of points based on the point's print format.

Edit the point and change the format from ###.### to ###.##

If the point is in a BACnet device edit the point under the BACnet Devices folder and set its format appropriately.