Reset the DX4700/DX4800 configuration settings to factory defaults.

Issue

How to factory reset the DX4700/DX4800 recorders.

Product Line

Pelco Video Management

Environment

  • DX4700
  • DX4800

Cause

Clear or reset the current configuration settings to factory default.

Resolution

To reset a DX4700/DX4800 to factory settings:

  1. Login with the admin user account.





     
  2. Click on the  Setup icon to enter the Setup menu.
     
  3. Select System.
     
  4. Click on Properties.
     
  5. Click Factory Default.
     
  6. Click on OK to confirm the DVR settings will be default to factory settings.