TAC Xenta 300 controllers without /N/P (networking and presentation) could be upgraded via the factory.

Issue

TAC Xenta 300 devices without /N/P (networking and presentation) could be upgraded by ordering an upgrade from the factory.

 Example of a 302/N/P label.                       Example of a non-/N/P 302 label.

 

Product Line

TAC Vista

Environment

TAC Xenta 301, TAC Xenta 302

Cause

TAC Xenta 300 controllers without the /N/P does not have functions for networking or to be connected to a presentation system, like TAC Vista.

Resolution

TAC Xenta 300 controllers without the /N/P could be upgraded to /N/P by following the process described in the attached datasheet.