How to display a wider screen view of live video from the IMP219.

Issue

How to increase size width of video screen for web page display

Product Line

Pelco Cameras

Environment

  • IMP219
  • IMP319

Cause

Black Bars displaying along opposite edges of the IMP219 camera web page view. 

Resolution

  1. Connect to the Sarix IP camera through IE web browser.
  • Click the Login option and login as admin for Username and admin for Password
  • Click on the Settings option.
  • Move pointer over AV Streams and select Video Configuration.
  • Clear out Primary and Secondary Stream settings.
  • Set Primary Stream H.264 Compression standard and set Resolution
  • Save/Exit.

The following two screen shots are only as an example to the differences between the two different Resolution settings.