Alarm email is not sent out and is discarded

Issue

Alarm email is not sent out and is discarded. The Last Discard Cause is 'BOutgoingAccount could not dequeue in-memory email: 501 Syntax error in parameters or arguments'. 

Product Line

TAC I/A Series

Environment

I/A Series G3

Cause

'Reply To' field in the Outgoing Account properties was left empty. This field specifies the contents of the 'From' field in the email that is sent.

Resolution

Configure the Outgoing Account 'Reply To' field with a valid email account. In the example below (G3 version 3.7), the valid account being used is my.account@gmx.com.