Issue
"Root element is missing" error window come up when attempting to edit a personnel object using the Personnel Manager.
Environment
CyberStation
Cause
Corrupted Personnel Manager data file.
Resolution
- Navigate to the Continuum installation folder.
- Locate the file "PersonnelEditorWorkstationSettings.xml"
- Edit the file and try to identify and fix the problem, if not able to identify/fix the problem you can delete the file but you will lose any customizations done to the personnel manager that are saved in the file such as the default location of area link schedules etc.