How do you prevent alarm popup from take over the DS ControlPoint screen?

Issue

The alarm popup interfere with search playback on control point.

Product Line

Pelco Video Management

Environment

  • Digital sentry
  • DSSRV
  • Control point

Cause

Ds system communicating a variety of messages to DS ControlPoint while running.

  • Information messages
  • Warning messages 
  • Critical messages. 

Resolution

Setting  "Alarm Popup" not to interfere with user but still allow alarm events to be manage.  

  1. Select "Setup" icon   located on the upper left corner.
  2. Select "Alarm Popup" menu .
     
  3. Select "Do not create tab or windows"


     
  4. Click on "Return to Setup
     
  5. Select the Live tab.
     
  6. Select the "Alarm Page" icon  to manage any alarm events.