Spectra IV Pendant Environmental parts

Issue

What are the part numbers for various components to the Spectra IV housing?

Product Line

Pelco Cameras

Environment

  • BB4T-PG-E
  • BB4-PG-E
  • BB4-PSG-E
  • BB4HD-PG-E

Cause

Analog Spectra IV Parts Inquiry

Resolution

The following images and part numbering are subject to change without notice. It is recommended to
consult with Pelco Technical Support for most current part numbers.

 

 Note: PA30-0150-6000G is now replaced by PA30-0150-6001G

Related Lessons Learned Articles:
Spectra IV door panel part number and components BB4DOORASSY
Spectra IV captive screws to secure lower dome
Spectra IV components. Dome Drive, Back Box, Lower Dome