What is the Main fuse value of the MCS16-10E

DANGER

HAZARD OF ELECTRIC SHOCK.
Remove all power from all devices before removing any covers or doors of the system. Disconnect the power at the device and at the power source.

Issue

Main Fuse value (amp) for the MCS16-10E

Product Line

Pelco Transmission & Power

Environment

  • MCS16-10E
  • MCS4-2E
  • MCS8-5E
  • MCS16-20E

Cause

Fuse value for replacement

Resolution

The Main fuse values are according to Table B below:

  • Installation Manual may be viewed here: C655M-A
  • Specification Sheet may be viewed here: C655
  • Note: The MCS*E series has been discontinued.