Precautions when upgrading MicroNet 100 series to MicroNet 50 series controller.

Issue

When a MicroNet 100 series LON controller is upgraded to a MicroNet 50 series LON controller, reference in/out objects and the bindings to the LON SNVT bindings are lost .

Product Line

Satchwell MicroNet

Environment

VisiSat Software version 2.1 Builds 137, 148, 148 SP1, 185 and 196.

Cause

The upgrade process removes various items/objects from the original scheme.

Resolution

The upgrade process removes various items/objects from the original bubbleland scheme.

Click here to view more detailed information.

 

Updated January 2014.
The MicroNet 50 series range MN350,450,550,650 LCD and Touchscreen have been withdrawn from sale.
Currently no direct replacement is offered.
The IAC 420, 600 and Touchscreen are not effected and remain available.