Can DS ControlPoint export video using the EXE format when connecting to DX Series recorders?

Issue

Using DS ControlPoint as the client software connecting to a DX4800 recorder, when exporting video will the EXE format work on any PC when played back.

Product Line

Pelco Video Management

Environment

  • DS ControlPoint 7.5.609 -7.12
  • DX8100/DX8000
  • DX4700/DX4800
  • DX4500/DX4600
  • DX4100
  • EXE
  • DS Media Player
  • XPA

Cause

Video export format which will playback on any PC without installing extra software.

Resolution

Yes, exported video using the EXE format includes the DS Media Player and video clip in a single .exe file.  To start playback double-click the exported .exe file.

 

Related Articles:
How do I export video or an image directly to CD/DVD using DS ControlPoint?
Can you Digital Zoom an exported video clip in DS Media Player?