Automation Server CPU Specifications

Issue

Automation Server CPU Specifications

Product Line

SmartStruxure Solution

Environment

SmartStruxure Automation Server version 1.4 and earlier

Cause

Automation Server CPU specifications is required for project submission. The Automation Server datasheet provides only basic information about the CPU. 

Resolution

The Automation Server uses the ATMEL AT91RM9200 microcontroller. This incorporates a ARM920T processor. You can download the datasheet here.

Note: The CPU in the AS runs at 160 MHz as this gives us optimal performance for our implementation. The component is however rated for a maximum of 180 MHz.