Issue
Is it possible to use the VF208W valve in applications with a glycol content up to 50%?
Environment
VF208W
Cause
Some valves are not suitable for use in applications with glycol content in media.
Resolution
The VF208W can be used in applications with deaerated water with glycol-type antifreeze agent (max 50%)