How to virtual PTZ an Oncam Grandeye 360 video export clip (.exe).

Issue

Virtual PTZ an exported video clip.

Product Line

Pelco Video Management

Environment

  • All Digital Sentry Product (version 7.6.32 and higher)
  • DS ControlPoint software (version 7.6.32 and higher)
  • Oncam Grandeye .exe
  • EVO Series all models

Cause

Information on playing back (.exe) Oncam Grandeye 360 video export clip.

Resolution

 
  1. Double click the .exe file to open and play.
  2. Move the mouse wheel forward or back to zoom in or out on a object.


     
  3. Click and hold the left mouse button, and then drag the mouse pointer in the direction you want to move the view.


     

Note: When using DS ControlPoint version 7.5.609, the exported video clip is unable to dewarp and zoom in on the image unless the PC being used has DS ControlPoint version 7.5.609 installed.  It is recommended to upgrade any PC running ver 7.5 .609 to 7.6.32 or later in order to export transportable video clips to be played on other PC without requiring DS ControlPoint to be installed on those machines.

Related Articles:

Where can I download the latest version of DS ControlPoint client software?