Can a 7716 emulate a 78061 Tap?

Issue

Can a 7716 emulate a 78061 Tap?

Product Line

TAC I/NET

Environment

I/NET site

Cause

Can a 7716 emulate a 78061 Tap?

Resolution

Yes, a 7716 can emulate a 78061 Tap.

Using the Hand Held Console (HHC):

  1. Press [Code], 90, [Enter]
  2. The emulated device type model number displays in the read out
  3. Press [Inc] or [Dec] to toggle through 7801, 7803, or 7806 Tap emulation
  4. Press [enter] to accept your choice
  5. You will need the RS 232 expansion card for ADAA

See TCON 096 for details