Unable to save a OGC Standard graphic page in vista 5.1.x

Issue

When you edit a OGC standard graphic and then attempt to save you get the error "Cannot save graphic object. Cause: FILE-service not available"

Product Line

TAC Vista

Environment

Vista 5.1.x

Cause

The OGC standard graphic does have this unknown issue on some sites.

Resolution

To allow the edit of the OGC edit the standard graphic and save out of the database.

The open with the OGC editor and make the changes that are required and save back into the vista database.