Activate the Windows 7 operating system utilizing Microsoft’s automated phone service

Issue

DSSRV is unable to active Windows 7 operating system online  

Product Line

Pelco Video Management

Environment

  • DSSRV
  • Windows 7

Cause

  • Lack of internet access prevents DSSRV from activating Windows 7 operating system online  
  • Copy of windows is not genuine

Resolution

Utilize Microsoft’s automated phone service to active the Windows 7 operating system 

To start the Product Activation Wizard, follow these steps:

1.      Click Start



2.      Right-click Computer.
3.      Select Properties.
4.      At the bottom of the window, click Activate Windows now.

In the Product Activation Wizard, follow these steps:

  1. Click Use the automated phone system to activate


     
  2. Click the drop-down menu, select the location that is nearest to you, and then click Next.


     
  3. The Product Activation Center telephone number is displayed under Step 1

  4. Follow automated phone system to complete Windows 7 operating system activation

Note: Product ID located on infront panel  inside the front cover