Where can I download the bin file player that comes with a native export when exported from a DX8100.

Issue

The bin file player crashes when native export camera from 17-32 are played.

Product Line

Pelco Video Management

Environment

  • DX8132 Series
  • Native video Export
  • DX8100 Viewer (bin file player) 

Cause

The older version of the bin file player had software issue.

Resolution

Download a newer version for the bin file player.

Click here to download DX8100 Viewer (DX8100 bin player.)

  1. Unzip DX8100 bin player.
  2. Open DX8100 bin player folder
  3. Double click DX8100V.exe
  4. Select folder icon on the DX8100 viewer and browser to video file that needs to be review.