Issue
SmartStruxure integration to Network 8000 - Supported Network 8000 devices
Environment
SmartStruxure Automation Server version 1.2 and above
Network 8000
Cause
Need to know the supported devices for a Network 8000 to SmartStruxure upgrade.
Resolution
Building Operation supports the following Network 8000 LCM devices:
- LCM
Building Operation supports the following Network 8000 ASD devices:
- Microzone II
- MicroFlo II
- LIM
- PEM
The following Micronet 2000 products are supported:
- MN-FLO
- MN-FLO3T
- MN-HPFC
- MN-ASDI
The following Network 8000 products are not supported in Building Operation:
- CCL GCM
- LNC
- SIM GCM
- PLC