Where to connect the Input Power of the EH1512 Series Enclosures.

DANGER

HAZARD OF ELECTRIC SHOCK.
Remove all power from all devices before removing any covers or doors of the system. Disconnect the power at the device and at the power source.

Issue

Where to connect 24VAC input power to the EH1512-2 enclosure?

Product Line

Other, Pelco Cameras

Environment

  • EH1512-1 (120 VAC power input)
  • EH1512-2 (24 VAC power input)
  • EH1512-3 (230 VAC power input)

Cause

Power Input wiring to the EH11512 series enclosures.

Resolution

For the EH1512 Series, the INPUT terminals serve as the connection point for Power Input. Refer to Figure 5 for each voltage models wiring connection.