Issue
How to i start a programmed pattern with KBD300A,KBD200A, KBD4000 or KBD4002
Product Line
Pelco Cameras, Pelco Matrix
Environment
- KBD300A
- KBD200A
- KBD4000
- KBD4002
Cause
How do you Initialize a pattern that is programmed in the camera with KBD300A, KBD200A or KBD4000
Resolution
- Select the camera you wish to run a pattern for.
- To run a pattern, press the pattern number (example 1) and then press the pattern button quickly don't hold the pattern button down.
- To stop the pattern move the joystick on the KBD300A or KBD4000 to stop the pattern on KBD200A or KBD4002 press a pan/tilt button.