How do I reset the Spectra II to default?

NOTICE

DISCONTINUED PELCO PRODUCT.
This product has been discontinued. For further information please visit pelco.com/support/discontinued-products

Issue

Reset Camera of the Spectra II 

Product Line

Pelco Cameras

Environment

  • Spectra II
  • SD5BC
  • SD5AC
  • DD5BC
  • DD5-C

Cause

  • Iris, Focus, Zoom is not automatically responding to changes
  • Settings returned to default value when RESET CAMERA is performed

Resolution

The Reset Camera feature restores the following options when the reset is performed.

View the following lessons learned article for menu access: "Access The Spectra Main Menu (Preset 95)          

 


Note: A Reset Camera is recommended should the Camera Optics features (iris, zoom, focus) not respond properly.