LED number 8 is always illuminated or in alarm state

Issue

LED number 8 is always illuminated or in alarm state.

Product Line

TAC I/NET

Environment

I/NET Controller

Cause

It means one or more points are, or were in alarm.

Resolution

This can be reset by the HHC. If the all points have return to normal, press ALARM ACK on HHC. Press ALARM SUMRY