TC300 thermostat cooling only operation

Issue

In applications where heating is not required is it possible to change the thermostat operation to cooling only?

Product Line

Field Devices

Environment

TC300

Cause

By default the TC300 thermostat is configured for heating and cooling. It should be possible to lockout operation of heating in cooling only applications so that the user cannot inadvertently change modes.

Resolution

In thermostat model TC303-3A2DLS parameter item 7 allows selection of cooling or heating only mode.