How do I change the order in which cameras appear on the DX4700/DX4800 main monitor display?

Issue

Would like to rearrange the camera order on the DX4700/DX4800 main monitor display.

Product Line

Pelco Video Management

Environment

  • DX4700
  • DX4800

Cause

The cameras are not displayed in the proper or desired order within the multi-channel display.

Resolution

  1. Log in as an administrator user
    • Default username = admin, password = admin
  2. Click the setup icon in the on-screen toolbar
    • If the on-screen toolbar is not displayed, right-click the mouse to bring it up
  3. Select the Display icon
  4. Select the Channel Assignment section
  5. Click the Name box for a channel
  6. Right- or left-click the Name box to select an entry
  7. Repeat the previous steps (as necessary) to configure additional channels
  8. Click Close
  9. Click OK

 

 

 

Related Articles:
How to switch between VGA and analog BNC monitors on the DX Series DVRs and HVRs recorder.
What display modes are available on the DX4700/DX4800 Spot Monitor output?