The PTZ function is lost after updating the NET5404T to 1.9.2.4

Issue

After updating the NET5404T to 1.9.2.4 it will lose PTZ function

Product Line

Pelco Cameras, Pelco Video Management, Pelco Transmission & Power

Environment

NET5404T, when updating to 1.9.2.4

Cause

This is a firmware bug

Resolution

After the update is complete reboot the NET5404T and the PTZ function will resume