Script program status is Loading after upgrade

Issue

Script program status is "Loading" after upgrade

Product Line

SmartStruxure Solution

Environment

Upgrade Script Program

Cause

A new keyword may have been added to the new version

Resolution

A new keyword may have been added to the new version, for example the word "Debug" can be used as internal variables in script programs up to v1.3, but not in v1.4 onwards. In this case simply change the word "Debug" to Debug1" and all works fine.

Screenshot of Script Properties shown below: