What is the part number for the CM9700 RJ-45 Sercomm Card?

Issue

No available RJ-45 ports

Add additional RJ-45 ports to the CM9700-CC1

Product Line

Pelco Matrix

Environment

CM9700-CC1

Cause

All of the ports are occupied by equipment

Expansion of devices

Hardware failure

Resolution

Part number - CM9700-SER