M-bus device template for Multical 602 to use in Xbuilder

Issue

Need a M-bus device template for Multical 602 to use in Xbuilder

Product Line

TAC Vista

Environment

Vista 5.1.8
Xbuilder 5.1.8

Cause

an Xbuilder device template for Multical 602 is required to integrate it with a Xenta Server (such as Xenta 913)

Resolution

Here is a M-bus device template for the Multical 602