How to Setup a FT85011 Transmitter and FR85011 Receiver to a KBD300A and DX8000/DX8100 DVR/HVR recorders.

Issue

No PTZ communication to my Spectra IV's thru the DX8000, KBD300A, and FT85011 transmitter and receiver

Product Line

Pelco Video Management

Environment

  • DX8000/DX8100 HVR/DVR recorders
  • KBD300A Keyboard (all versions)
  • Spectra IV

Cause

Wiring from the KBDKIT to the FT85011 transmitter was incorrect.

Resolution

For more information on physical wiring installation of the KBD300A and DX8000/DX8100, please refer to article Default settings and wiring needed in order to control Spectra IV from a DX8000/DX8100 Series HVR

For more information on KBD300A keyboard functions, please refer to article "What are the KBD300A keyboard function keys when connected to a DX8000/DX8100 HVR"