DS ControlPoint full screen mode expands beyond a single monitor when used in a multi-monitor configuration.

Issue

  • DS ControlPoint full screen mode expands beyond a single monitor when used in a multi-monitor configuration.

DS ControlPoint Bleed Over

 

  • A single camera screen display show other camera in the same screen.


     

Product Line

Pelco Video Management

Environment

  • DS ControlPoint
  • Windows 7
  • Windows XP

Cause

Using medium to large fonts in Windows 7 as well as using fonts larger than 96 DPI in Windows XP.

Resolution

Windows 7

  1. Right-click on the Desktop
  2. Click Personalize
  3. Bottom left hand corner of Personalize screen click Display
  4. Click Smaller - 100%
  5. Click Apply
  6. Select Log Off Now
  7. Log back into Windows
  8. Re-launch DS ControlPoint

 

Windows XP

  1. Right-click on the Desktop
  2. Click Properties
  3. Under Properties click Settings
  4. Under Settings click Advanced
  5. At the General Tab set DP Setting to Normal (96 DPI)
  6. Click Apply
  7. Reboot Windows
  8. Re-launch DS ControlPoint