Issue
A jobsite consists of several (independent) buildings each installed with a UNC-520. They are not networked together (i.e. standalone) and each one has a different projectID. The customer would like to use Workplace Pro to do some occasional changes and scheduled database backups. Can a copy of Workplace Pro be purchased / provided without the need to purchase the Enterprise Server as well?
Environment
Niagara R2
Cause
Unusual jobsite configuration with several standalone UNC-520 controllers and no Enterprise Server.
Resolution
Workplace Pro can only be purchased along with the Enterprise Server software. It cannot be purchased in any other configuration.
Perhaps an arrangement can be made with the local Schneider-Electric branch or I/A partner for temporary usage of a pc with Workplace Pro.