TAC Xenta I/O modules as Stand Alone LonWorks device

Issue

What TAC Xenta I/O modules could act as Stand Alone LonWorks device?

Product Line

TAC Vista

Environment

TAC Xenta 420A
TAC Xenta 421A
TAC Xenta 422A
TAC Xenta 450A
TAC Xenta 451A
TAC Xenta 452A
TAC Xenta 410
TAC Xenta 411
TAC Xenta 412
TAC Xenta 420
TAC Xenta 421
TAC Xenta 422
TAC Xenta 450
TAC Xenta 451
TAC Xenta 452
TAC Xenta 470
TAC Xenta 471
TAC Xenta 490
TAC Xenta 491
TAC Xenta 492

Cause

It is only TAC Xenta 421A, 422A, 451A and 452A that could act as Stand Alone LonWorks devices.

Resolution

It is only TAC Xenta 421A, 422A, 451A and 452A that could act as Stand Alone LonWorks devices.

TAC Xenta 400 I/O modules without -A, will not work as Stand Alone LonWorks devices.