Bacnet Network ID-UDP setting explained

Issue

What is the BACnet Network ID - UDP

Product Line

Andover Continuum

Environment

bCX4000

bCX4040

Cause

Documentation

Resolution

The BACnet Network ID - UDP identifies the network on the Ethernet that the bCX controller is sitting on, it is 1 by default.

Note that the CyberStation does not have a setting for BACnet Network ID - UDP, CyberStation will communicate with all ethernet level BACnet devices regardless of the network they sit on.