Issue
Pin point crash issue:
• Pinpoint crash
• Scroll bar does not work on upgrade from older revisions of CyberStation
• Making changes to a graphic created in Pre 1.94 CyberStation causes the graphic canvas size to become corrupted
• Copying objects/controls of a graphic and pasting them to the same graphic causes the graphic canvas size to become corrupted
WebClient DMZ issue:
This hotfix corrects an issue where web.Client positioned in the DMZ only communicates in one direction.
Web Client Personnel Area issue:
This hotfix corrects an issue where the web.Client IE browser PC becomes disconnected from the web.Client server when attempting to remove area(s) of personnel objects. It also corrects an issue with web.Client not removing area(s) if the personnel records are not re-opened after saving.
Environment
Windows all versions
Continuum 1.94 SP1
Web Client
Cause
This is due to bugs which have been discovered and have now been fixed
Resolution
Please go to the below link for hot fixes that apply to your problem, there is also a complete install pack of SP1 which includes all hot fixes which should be installed if SP1 has not already been applied