Picture goes out of focus when the lower dome is installed on a IE30DN-1

Issue

Picture goes out of focus when the lower dome is installed on a IE30DN-1

Product Line

Pelco Cameras

Environment

  • IEE10DN-0 IEE10DN-1 IEE10DN8-1 
  • 13M2.2-6 13M2.8-8 13M2.8-12 13M15-50 
  • IEE20DN-1 IEE20DN8-1

Cause

13M15-50 lens while mounted on the IE30DN-1 and then install the lower dome

Resolution

To focus:

  1. Hold the dome in front of the 13M15-50
  2. Adjust the focus of the lens 

This should provide a focused picture when the lower dome is attached.