What is the difference between a CM9770-DFC card and a CM9770-DFL?

Issue

CM9770 down frame card options

Product Line

Pelco Matrix

Environment

CM9700-CC1

CM9770-MXB

CM9770-DFC

CM9770-DFL

Cause

Adding additional monitors and cameras to a CM9700 matrix.

Resolution

  • CM9770-DFC - This is the "no looping" downframe card.
  • CM9770-DFL - This is the "looping" downframe card.