Does the Sarix IME119 feature image rotation?

Issue

Does the IME Series and IXE Series Sarix cameras feature image orientation?

Product Line

Pelco Cameras

Environment

  • IME119 series
  • IXE Series
  • IME Series

Cause

 Mounting the IME119 upside down per installation requirements.

Resolution

Sarix Image Orientation may be edited per installation requirements.

Configuring the orientation of the scene:

  1. Place your mouse pointer over the Imaging tab
  2. Select General from the drop-down menu.
  3. Select one of the following options:
    * Click the "Flip left-to-right" box to rotate the camera image 180 degrees horizontally.
    * Click the "Flip top-to-bottom" box to rotate the camera image 180 degrees vertically.
  4. Setting is automatically saved when page is exited.

View a snap shot of image flip option here: Image Orientation

 

Manual IME119 page 22 C2270 (7/13).