At what temperature will the heaters turn on for the Spectra IV camera.

Issue

At what temperature will the heaters turn on for the Spectra IV camera.

Product Line

Pelco Cameras

Environment

  • Spectra IV
  • Heater/Blower

Cause

What is the Spectra IV normal operating temperature.

Resolution

The Spectra IV PTZ camera will run around 70 degrees. Heaters and blowers will automatically run to maintain this temperature.

Spectra Series Operating Temperature:

Surface Mount / Indoor In-Ceiling  0°C / 32°F  50°C / 122°F
Standard Pendant*  -4°C / 25°F  45°C / 113°F
Environmental In-Ceiling / Pendant*  -51°C / -60°F  60°C / 140°F
Pressurized & Stainless Steel  -51.11°C / -60°F  60°C / 140°F
Heavy Duty In-Ceiling  32°C / 0°C  50°C / 122°F
Heavy Duty Pendant  32°C / 0°C  60°C / 140°F
Heavy Duty Environmental Pendant  -51°C / -60°F  60°C / 140°F
Spectra Mini  0°C / 32°F  50°C / 122°F

All values assume no wind chill factor.
* Horizon Series

Note: The heater and blowers are pre-programmed and cannot be adjusted.