What is the CM9700-CC1 Floppy Drive part number?

Issue

The floppy drive will not read a disk.

Error reading drive A:

Product Line

Pelco Matrix

Environment

CM9700-CC1 Floppy

Cause

Hardware failure

Resolution

The replacement part number for the CM9700-CC1 Floppy Drive is - EE05-0111-1200G