Issue
What is the part number for the Din-rail adapter plate?
Product Line
Pelco Transmission & Power
Environment
- FMCI-AF1MM1ST
- FMCI-AF1SM1ST
- FMCI-BF1SM1ST
- FMCI-BF1 MM1ST
- DINBKT1 (Purchased through COMNET)
Cause
Requesting Din-Rail mounting option for Pelco Fiber Modules
Resolution
Pelco by Schneider Electric currently does not offer a Din-rail mounting option for the listed fiber modules. A compatible Din-Rail kit may be purchased through COMNET if part is required.
Comnet part numbers are as follows:
- DINBKT1 - Pelco to DIN Rail Adaptor Plate, with mounting hardware kit
View the attached Comnet Specification sheet for further product and purchasing information: DIN RAIL sheet