Installation details for the SPW100 range of sensors required

Issue

Where can additional information on the SPW100 series differential pressure switches be found.

Product Line

Field Devices

Environment

SPW100, SPW102, SPW104,SPW106, SPW108, SPW110, SPW114

Cause

Only the Schneider Electric datasheet and CE declaration are posted on the Extranet, no installation documents are available.

Resolution

Attached are the OEM suppliers datasheet and installation guide along with the Schneider Electric documents.

Download here.