Issue
The drop down menu to select WorkPlace Tech help manuals does not function in Internet Explorer 11.
Product Line
TAC I/A Series, SmartStruxure Solution
Environment
WorkPlace Tech 5.8.6
Internet Explorer 11
Cause
Internet Explorer changes how they handle compatibility mode for websites and webpage used to access the help files requires updating in a new version of WorkPlace Tech.
Resolution
Use one of the following options to access the help files
- Access them directly by going to the folder they are stored. On a Windows 7 (64 bit) operating system this is C:\Program Files (x86)\WorkPlace Tech\Help by default.
- Modify the index.htm, BACnet.htm, LON.htm, search.htm, Sensors.htm, and Software.htm files found in the C:\Program Files (x86)\WorkPlace Tech\Help\bin directory.
Add the following line in front of the first "meta http-equiv=" line: